Key Features

Kollmorgen Automation Suite is Kollmorgen an all-in-one solution for designing, developing and maintaining automation systems. It integrates the three main functionalities of a machine:

KAS IDE

KAS comes with a powerful Integrated Development Environment (IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger) which allows you to:

Main Tools

Tool Description
Pipe Network Editor Graphical tool describing the mechanical System into the logical world based on an one to one translation
Cam profile Editor Allows you to create or modify a profile definition that describes the position evolution of the cam in a 2D graphical format
Softscope Allows to view in a two-dimensional graph one or more variables' evolution (vertical axis) across the time (horizontal axis)
Simulator Allows you to develop your application without any hardware available

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen